Register iFIX Plug-in with Configuration Hub
Use these steps to register the iFIX plug-in with Configuration Hub after Webspace is installed.
To register iFIX with Configuration Hub. On the Configuration Hub machine, follow the steps in the Configuration Hub Registration topic.
Be aware that before registering iFIX with Configuration Hub, you need to:
- Enable security on all iFIX SCADAs. See Enabling or Disabling Security.
- Be aware that the Configuration Hub web server and the iFIX plugin ports must be allowed in the firewall exception rules during installation. If you do not do this during installation, you will need to add these applications manually to the firewall rules.
- If you are using Configuration Hub on a domain, you may need to update the HOSTS files on your network with the name of the Configuration Hub server, the iFIX SCADA Server, and Historian Server (if applicable).