Interactive Map
This topic describes properties for an interactive map layout.
The interactive map functionality is available in both coordinate and flexbox card layout types. For older version, see Interactive Map.
- Upload an image.
- Double-click the image areas where you want to create a marker.
- Select the marker you want to update.
- On the details panel, select +Add Marker State, and update the properties.
- Similarly update all markers on the image.
- You can also delete markers on the image.
Field Name | Description |
---|---|
Map Image | Select Upload Image to browse and select an image. The option to upload an image is also available within the interactive map card layout. |
Coordinates | Enter these coordinates to position the image within the card. The value
should be less than or equal to 99.
You can also set the coordinates by moving the image on the layout. The values in the text box are adjusted based on the set position. |
Marker Type | You can select one of the following options:
|
Color | If you selected Shape as the marker type, specify a fill color. |
Shape | If you selected Shape as the marker type, select
one of the following options:
|
Marker Image | If you selected Image as the marker type, upload
an image for the marker. For example, if the marker identifies the position of a radiator fan, you can upload the image of a fan instead of using a predefined round or square shape for the marker. |
Size | Enter the size to multiply the default size of the marker shape or image
size. For example, if you enter 2, the marker size is double the default size. By default, the value in this field is 1. The marker size can have a value greater than or equal to 100. |
Label | If you want a label to appear for the marker, then enter the label name. |
Label Color | Choose a color for the label text. |
Data Label | You can choose to pass the data to the interactive map using a query,
global, formula, or enter the value manually. For example, suppose the interactive map plots the temperature of various components of a car. For a marker that identifies the position of a radiator fan in a car, you can map the data label with the output of the query that retrieves the temperature of the fan. When you access the application, the temperature value retrieved from the query is displayed for the radiator fan. |
Number Format |
|
Data Label Color | Identifies the color and opacity of the data label. |
Show/Hide | Select +Add Conditions to create conditions that show or hide the interactive map. See Apply Conditions. |
BEHAVIOR | You can set actions to be performed when a marker is selected.
|
Delete Marker | Select the marker you want to delete, and select the Delete icon. |