Edit Graphic

This topic describes how to modify a HMI graphic.

About this task

You can modify custom HMI graphics only.

Procedure

  1. Under Custom plug-ins, right-click the graphic you want to modify.
  2. Select Edit Graphic.
    The graphic opens in an SVG editor.
  3. On the components panel, access the following tabs to modify the graphic:
    Graphic Tree On this tab, you can view the hierarchy of SVG elements and corresponding animations. You can add or delete animations from this tree only. Refer to the following topics:
    Graphics List On this tab, you can access all the plug-ins listed under the custom category. Refer to the following topics:
  4. Save the changes made to the graphic.

Results

Note: Modifying graphic templates in an application affect the rendering of data and animations in the runtime environment. You need to manually replace the instances of the graphic template with its latest version in all affected pages. Refer to the table:
Graphic Template Modifications What To Do
Added new animation Update graphic instances to see the new animations.
Deleted existing animation Update graphic instances to reflect the changes.
Modified visual elements (adding shapes, changing colors, etc.) No manual action required. Changes are automatically recognized by graphic instances in the runtime.