Dropdown
Allows to use standard features of a dropdown.
A dropdown is a graphical user interface element that allows a user to select one option out of a set of predefined options. Dropdowns are characterized by a wider set of options than that of a radio button. Radio buttons rarely have more than three options, while dropdowns can contain many more options. For advanced features, use the multi-feature Dropdown.
Dropdown Properties
Field Name | Description |
---|---|
Required | Select the check box to send the input to the query. |
Target Data | The target data defines where the information will be sent. |
Options | Dropdowns require multiple options that are mutually exclusive. Use
these available options to populate dropdown list items:
|
Data | Select this option if you want to provide data by means of a query output or a global parameter. |
Manual | Select this option if you want to manually provide data. |
Submit on change | Select the check box if you want to submit the query whenever the input value is updated. |
First Option | By default, the first option in a dropdown is blank. It is recommended to manually enter option text such as please select, instead of a dropdown that appears empty. Enter its option value to be none. |
Possible Uses
Dropdowns are similar in nature to radio buttons in that they require a mutually exclusive selection. However, while radio buttons are generally used for options between only a few choices, dropdowns can include hundreds of choices. One example of a drop-down list box could be selecting a country of residence. Every country in the world will take up too much space if displayed as radio buttons, while in a drop-down list box, the information can be more elegantly contained. The information selected could be converted to other information depending on the target data. For example, the country could be changed to a telephone prefix by setting the value to be telephone prefix and the display as the country name.
- Drag-and-drop the dropdown widget to a container.
- Select the dropdown widget in the container to access the DROPDOWN PROPERTIES tab
- Under the GENERAL section, provide the details as
specified in the table:
Field Name Description Label Enter Select an option. - Under the DATA section, provide the details as
specified in the table:
Field Name Description Target Data Select a query. Options Select Dynamic. Value Select PREF. Display Select PREF. Submit on change Select the check box.
In the practical application, a query can be executed based on the option selection in dropdown and the facility or company status in the prefecture can be displayed on a map as markers.