Map
This widget is available only in Operations Hub Classic version.
A map widget is used to display a map in an application. It uses the Google Maps feature. You can use the map widget to display the location of a place on a map (for example, the location of each site of a company).
To display asset locations on the map, you must access the API key generated by Google.
Map Properties
Field Name | Description |
---|---|
Label | Identifies the title of the map. |
Display | Identifies the type of the map. You can select one of the following
values:
|
Layers | Identifies the layer that you want to display on the map. You can
select one of the following values:
|
CENTER | Identifies the center point of the map. You can specify the center
point using one of the following sources:
|
MARKERS | Identifies the markers that should appear on the map. Select Add Marker, and then enter or select values in the following sections or boxes that appear. See Markers table. |
SHAPES | Identifies the circle that covers the area of a location. For
example, if the map displays the locations of sensors that capture the
radio signals within a radius of 1 km, you can add a shape to each
marker to indicate the area covered by each sensor. Select Add Shape, and then enter or select values in the following sections or boxes that appear. See Shapes table. |
Field Name | Description |
---|---|
Position | Select one of the following options:
|
Label | Select one of the following options:
|
Marker Icon | Select the icon and color of the marker. |
Condition | Select Add conditions, and then specify the
conditions for displaying the marker. Tip: You can add
multiple markers. For example, if you want one marker to represent
sites whose overall plant efficiency is above 95 percent and another
marker to represent sites below 95 percent, you can add the two
markers with the same position data, and specify the conditions
appropriately on each one. |
Actions | Select Add Action, and then specify the action that should be triggered when the marker is selected (for example, display more details about the location). |
Field Name | Description |
---|---|
Position | Select one of the following options:
|
Radius | Select one of the following options:
Note: The radius can also be used as a visual indicator of other
parameters, such as signal strength. |
Color | Select the color of the shape. You can also specify the opacity. |
Condition | Select Add conditions, and then specify the conditions. For example, if you want the marker to represent the signal strength received by a sensor, you can add multiple shapes with different colors and the same position data, and then specify different signal strength conditions on each shape. |