Update Plug-in Version

This topic describes how to update the version number for custom plug-ins.

Use the following format to update a plug-in's version number: MAJOR.MINOR.PATCH. Suppose a version is updated from 1.0.0 to 1.0.2, then 1 stands for major version, 0 stands for minor version, and 2 refers to patch updates. For more information, refer to the versioning policy in the following table:
Version Update When
MAJOR You made major schema changes, which are incompatible with the previous version. For example, modifying existing fields in a plug-in.
MINOR You added/removed a field. For example, including or deleting source/target fields in a plug-in.
PATCH You resolved backward compatibility issues. For example, bug fixes for customer cases.

MAJOR or MINOR Update

If the MAJOR or MINOR version of the plug-in is changed, then do either of the following:

PATCH Update

If only the PATCH version of the plug-in is changed, then the plug-in is automatically upgraded to the latest version.