Breadcrumb
With the Breadcrumb plug-in, you can navigate through the asset model.
Operations Hub New Layout | Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub. |
Operations Hub Classic Layout | Refer to About Widgets (Classic) |
The purpose of a breadcrumb is to allow you to access an asset's information located anywhere in the asset model hierarchy. A breadcrumb navigation also defines the relationship between different assets in a model.
The breadcrumb navigation is available for all the widgets in Operations Hub. You can navigate in the trend card using breadcrumb.
In the end application UI, to access the breadcrumb, select
and browse your model.



You must specify these breadcrumb properties:
Note: When configuring input targets for plug-ins, ensure that no other binding exists for
the target query input. To remove a binding from the query input, select the unlink icon
next to the binding.
Breadcrumb Properties
Field Name | Description |
---|---|
Source Asset Context | Select the source (asset name) for an asset context. The selected context
appears as a default breadcrumb view in the end application. This asset name
must exist in your asset
model.![]() |
Target Asset Context | Select the target for an asset context. This target defines where that
output goes on selecting an asset in a breadcrumb, so that it can be fed either
to a query or a global.![]() |
Target Extension Query for Asset Context Properties | Select the target for an extension query. This is a formatted string with
a list of properties that defines the hierarchy of the breadcrumb in the end
application. For example, consider these crumbs in a hierarchy - first is
‘pump’, second is ‘pump pressure’, ‘pump frequency’, ‘pump vibration’, or ‘pump
flow’. ![]() |