Pie Chart

Operations Hub New Layout Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub.
Operations Hub Classic Layout Refer to About Widgets (Classic)

Pie Chart Properties

Field Name Description
Pie Type Select from the available list of pie charts.
Source > Data Source Provide the input data source for the chart either manually or through data binding.
Note: If configuring data source manually, ensure that the first output field is always a 'value' and the second is a 'string'.

If binding data through drag-and-drop method, you don't need to do anything. The order of the fields is automatically handled.

Title Title name for the chart.
Subtitle Subtitle name for the chart.
Legend Select the Visible check box if you want to show the chart legend. You can also use the options to position the legend in the chart.
Show Labels Select the check box if you want to show labels in the chart.
Show Tooltips Select the check box if you want to show tool tips in the chart.
Show Name Select the check box if you want to show label name.
Show Value Select the check box if you want to show values in the tooltip.
Show Percentage Select the check box if you want to show percentages in the tooltip.
Hidden Select this check box if you want to hide the plug-in. To show the hidden plug-in in Operations Hub new layout, go to Page Visuals and under Action column, select for the hidden plug-in. See Page Visuals Tab.
Note: When exporting a chart to JPEG or PDF at runtime, make sure your browser's zoom is set to 100% or above.