Gauge Bar

Operations Hub New Layout Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub.
Operations Hub Classic Layout Refer to About Widgets (Classic)

Gauge Bar Properties

Field Name Description
Source > Input Value To get values for gauge bar from a data source, use any of these options:
  • Select a query output.
  • Select a global parameter.
  • Enter source data manually.
  • Add a formula.
Note: If configuring data source manually, ensure that the first output field is always a 'value' and the second is a 'string'.
Source > Minimum Value Sets the minimum scale value.
Source > Maximum Value Sets the maximum scale value.
Use Raw Format Select the check box to display numbers in raw format.

For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off.

Number of decimals This option appears if you do not want to display numbers in raw format.

In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number.

Advanced Settings
  • Select the Show Label check box to display a label name, if provided.
  • Select the Show Animation check box to display animation.
  • Select the Show Legend check box to display a legend.
Angles
  • Start Angle: Defines the point on the circumference of the gauge at which the bar will begin to appear in displaying the input value.
  • End Angle: Defines the point on the circumference of the gauge at which the bar will complete its appearance in displaying the input value.
Hidden Select this check box if you want to hide the plug-in. To show the hidden plug-in in Operations Hub new layout, go to Page Visuals and under Action column, select for the hidden plug-in. See Page Visuals Tab.

Bar Gauge at Runtime

Note: If you choose to show legend on a graph with large amounts of data values, the graph may become unreadable.