Gauge Circular

Operations Hub New Layout Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub.
Operations Hub Classic Layout Refer to About Widgets (Classic)

Gauge Circular Properties

Field Name Description
Source > Input Value To get values for gauge circular from a data source, use any of these options:
  • Select a query output.
  • Select a global parameter.
  • Enter source data manually.
  • Add a formula.
Source > Minimum Value Sets the minimum scale value.
Source > Maximum Value Sets the maximum scale value.
Use Raw Format Select the check box to display numbers in raw format.

For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off.

Number of decimals This option appears if you do not want to display numbers in raw format.

In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number.

Advanced Settings
  • Select the Show Label check box to display a label name, if provided.
  • Select the Show Animation check box to display animation.
  • Select a Needle Color.
  • Choose a Needle Style from available options - rectangle needle, triangle needle, range bar, marker, text.
Range(s) You can specify one or more ranges to display in different colors.
  1. Select +Add Item.
  2. Start of Range
  3. End of Range
  4. Select a color Color in Range.
Hidden Select this check box if you want to hide the plug-in. To show the hidden plug-in in Operations Hub new layout, go to Page Visuals and under Action column, select for the hidden plug-in. See Page Visuals Tab.

Circular Gauge at Runtime