Indicator

Use the indicator widget to monitor and interpret the status of your industrial systems.

Operations Hub New Layout Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub.
Operations Hub Classic Layout Refer to About Widgets (Classic)

You can apply different colors and introduce gif animations to communicate a value or state effectively. The indicator widget helps to draw attention towards the changing status of a system and the indication to take corrective actions, if necessary. For a simpler version, use Simple Indicator.

Bind the widget to a query and set the properties to appear at runtime. You can define unique properties for values within specific ranges, and also for values that are outside of any range.

Important: This rule applies if you have upgraded to a SIM version. Make sure to upgrade your applications before attempting to modify them in Operations Hub.

Indicator Properties

Field Name Description
Multistate Indicator Value The value is populated when you bind the indicator widget to a query.
Indicator Mode Select to display output in any of these modes:
  • Analog: In this mode, the widget provides analog values as output. You can choose to add a background image, and use several other options to indicate the current status.
  • Status: In this mode, the widget functions as a simple indicator status. It provides a push button to indicate the change in current status. You can also choose to show the analog values.
  • Image: In this mode, you can provide a background image to indicate the change in current status. You can also choose to show the analog values along with the image.
Display Value? Select the check box to display the analog value.
Repeat Background Image Analog indicator mode:

Select the check box to apply the background image repeatedly to provide a continuous background across the widget.

Width Analog indicator mode:

By default, the indicator widget occupies the width of its container. Reset the width in percentage or pixels.

Height Analog indicator mode:

By default, the indicator widget occupies the height of its container. Reset the height in percentage or pixels.

Size Image and Status indicator modes:

For the image mode, enter the image size in pixels.

For the status mode, enter the size to set the diameter of the indicator button.

Use Raw Format Select the check box to display numbers in raw format.

For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off.

Number of decimals This option appears if you do not want to display numbers in raw format.

In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number.

Insert Commas Select the check box to use comma as a thousands separator. A comma is inserted for every three digits.
Prefix Units Enter the unit of measurement to appear as a prefix for the value.
Suffix Units Enter the unit of measurement to appear as a suffix for the value.
Label Above Enter the text to appear above the value.
Label Below Enter the text to appear below the value.
Font Size Enter the size of the font for the label text.
Font Family Select a font family for the label text.
Font Color Select a font color for the label text.
Background Color Select a color to fill in the background for labels and values.
Background Image Mode Use these options to set a background image for the widget.
Type: If you choose to set a background image, then select from these two types:
  • File: Browse and select the file you want to use.
  • URL: Enter the complete URL address for the image from a server.
    Note: Applies to importing applications from an older version of Operations Hub Classic to Operations Hub 2023.

    When you import an App to v2023, the Indicator plug-in’s Background Image Mode > Type is altered in the new system.

    To rectify in the imported App, go to the Designer and select the Indicator plug-in to access its properties. Change the Type back to the originally set type. The original source information (if exists) is retrieved.

Background Image Fit: Determines how the image fits into its container, whether to align horizontal (or) vertical. Background Image Position: Determines the position of the image, whether the image should be placed behind value only, (or) behind value and labels.

Border Type: Select from different types of border styles to apply to the background image.

Border Width (Pixels): Enter the width size if the widget has a border.

Border Radius (Pixels): Enter the radius size to style the corners of a border.

Border Color: Select a color for the border.

+Add Item Select to customize settings for values within a specific range. Create an input range and highlight with unique colors and style.
Input Range Low (Greater than or Equal) Enter the lowest value to create an input range.
Input Range High (Less than) Enter the highest value to create an input range.
Hidden Select this check box if you want to hide the plug-in. To show the hidden plug-in in Operations Hub new layout, go to Page Visuals and under Action column, select for the hidden plug-in. See Page Visuals Tab.

About Custom Range Settings

You can add several custom ranges to the widget; each with a different input range. The custom ranges are implemented in the specified order, from first to last. If the input ranges overlap with each other, the custom range setting at the top of the order is applicable. Arrange the custom ranges in the order you want them to be implemented.
  • Select for the custom range to move upwards in a list.
  • Select for the custom range to move downwards in a list.
  • Select for the custom range to remove from the list. These inputs are deleted.