Spider Chart
Use spider charts to compare and analyze multiple data sets.
With the spider chart widget, you can:
- Create visually appealing spider graphs.
- Apply unique color coding for efficient comparison of data.
- Analyze values that change over a period of time.
- Use the resultant information for better decision-making.
Operations Hub New Layout | Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub. |
Operations Hub Classic Layout | Refer to About Widgets (Classic) |
Spider Chart Properties
Field Name | Description |
---|---|
Title | Enter a title name for the spider chart. The title appears at runtime. |
Font Color | Select a font color for the spider chart text. |
Line Color | Select a line color for the spider chart axes. |
Default Min | Enter the minimum axis value.
|
Default Max | Enter the maximum axis value.
|
Legend | Select:
|
Max-width | Enter the maximum width the spider chart can occupy in an application. |
Axis Labels | Add items to create multiple axes in a spider chart. Enter the following
information for each item (axis):
|
Series | Add items to set up a data series for the spider chart.
|
Hidden | Select this check box if you want to hide the
plug-in. To show the hidden plug-in in Operations Hub new layout, go
to Page Visuals and under
Action column, select ![]() |
Spider Chart at Runtime