Text Input

Use this plug-in to add a text box in your application.

Operations Hub New Layout Refer to Visuals Tab for more information on the layout of widgets in Configuration Hub.
Operations Hub Classic Layout Refer to About Widgets (Classic)

Text Box Properties

Field Name Description
Target > Output Value Provide the target data source to send information.
Source > Input Value Provide the input data source to receive values for the text box.
Use Raw Format Select the check box to display numbers in raw format.

For example, a numeric value with 5 or more decimal places is shown as it is, and not rounded off.

Number of decimals This option appears if you do not want to display numbers in raw format.

In that case, enter the decimal places (0-7) to consider after the decimal point to format large numbers. Based on the decimals, the value is rounded off to the nearest whole number.

The decimals will apply to Input Value, Minimum Value, and Maximum Value properties.

Display Mode Specify the input type for the taxt box, whether password, email or URL.
Enable Clear Field Action Select the check box to add a delete option in the end app to clear any data in the text box.
Label Styling Formats the text: Font Family, Font Size, and Font Color formats the text entered in the text box.
Hidden Select this check box if you want to hide the plug-in. To show the hidden plug-in in Operations Hub new layout, go to Page Visuals and under Action column, select for the hidden plug-in. See Page Visuals Tab.