Configure CIMPLICITY for Alarms
When using the CIMPLICITY HMI/SCADA system as your data source, follow this quick walkthrough to successfully get data and alarms flowing for the first time into Operations Hub.
Before you begin
- Install the latest versions of CIMPLICITY and Operations Hub on different servers or on the same server.
- Create an administrative user that you can use for both CIMPLICITY and Operations Hub. The user IDs must match in order to connect and manage communications and operations between the two systems, but the passwords must be different.
Procedure
- Start the CIMPLICITY Workbench application.
-
From the Workbench toolbar, go to
.The Create User for New Project dialog appears.
-
Provide these details for the new user account:
Field Description Username Enter the user name for the new account. Password Enter a password. Confirm password Enter the password again to confirm. Note: You will use the credentials to establish a secure connection with authentication for the CIMPLICITY data source in Operations Hub. -
Select Next.
The Create As dialog appears.
-
Enter the name and location for the new project.
Note: For write operations to work, the project name and the CIMPLICITY data source name in Operations Hub should be the same.
- Select product options and protocols that will be included in the project.
- Select Create.
-
After creating the project, go to
.The Project Properties screen appears.
-
On the OPC UA Server tab, perform these steps.
- Select the check box for Enable Server.
- Select Security Configuration, then select the check box for all the security options you want to enable for the OPC UA server.
-
On the Operations Hub tab, perform these steps.
- From the CIMPLICITY Workbench project directory, right-click , to create a new device point.
-
Provide the following information for the new point and select
OK.
Field Description Point ID Provide a unique name that identifies the CIMPLICITY point. Type Select Virtual. Class Select Analog. The Point Properties screen appears. -
On the Virtual tab, provide these details:
Field Description Initialization Select Initialized. Initial value Enter 0. Calculation Select Equation and build an expression. For more information on calculation types, refer to the Configure Virtual Calculations topic in the CIMPLICITY help guide. -
On the Alarm tab, provide these details:
Field Description Alarm message Select Point ID. For more information on alarm message variables, refer to the Enter an Alarm Definition topic in the CIMPLICITY help guide. Alarm limits Enter the alarm limits. For example: - HiHi: 60
- Hi: 40
- Lo: 20
- LoLo: 10
- Select OK to save and close the Point Properties screen.
- Repeat steps 6-10 to create more device points.
- Run the CIMPLICITY project.
What to do next
- Create a data source with OPC UA configuration in Operations Hub.
- Use the alarm card and alarm count widgets in your application.
- Acknowledge Alarms.
- Apply Filters to View Alarms.
- Configure iFIX for Alarms.