Create Extension Query (Classic)
This topic describes how to create an Extension query.
Before you begin
About this task
Procedure
-
In classic Operations Hub navigation menu, select
QUERIES.
The QUERIES workspace appears.
-
Select Add new query.
The New Query window appears.
-
Provide these details:
Field Name Description Name Enter a name for the new extension query. The name must contain at least one uppercase or lowercase letter. Type Select Extension. Additional options for creating the extension query appear.
Description Briefly describe the purpose of the query. Method Select the type of extension query you want to create from these options: - Read
- OPC UA Write
- Historian Add Comment
The sections Query Parameters and Output Data appear based on the method selected for the query.
-
Specify Query Parameters.
Refer to Extension Query Parameters.
-
Under the Output Data section, you can include one or more
output data fields to your extension query.
Following output fields are available to use:
Output Data Field Description Timestamp
This field represents the timestamp associated with each data point. Name
This field represents the tag name you want to query in the database. Value
This field represents the actual data value associated with the specified tag at a given timestamp. Quality
This field represents the quality of the data at a specific timestamp. Data Attributes
This field represents data attributes associated with the data point. Historian is now enhanced to store up to 128-bit quality types, which are stored in data attributes. These attributes are extended qualities that you can store more than the regular qualities and sub qualities such as good and bad. In addition to regular qualities, the HAB collector collects extended qualities such as replaced, suspect, garbage, old, and so on. You can use these attributes using REST APIs as well as Configuration Hub.
Select
next to the output data field you do not want to include in your query.
- Save the extension query.