This topic describes the uninstalling of Operations Hub.
About this task
To completely remove the Proficy product installation, you
need to uninstall the following applications as per the instructions that follow:
- Configuration Hub
- Operations Hub
- Proficy Authentication
Procedure
- If you want to uninstall Operations Hub automatically, open Command Prompt, and enter the following command:
<Installation folder path of Operations Hub>\OpHub-Windows_Installer>ophub_bundle -uninstall
-
If you want to uninstall Operations Hub
manually, perform the following steps:
-
On the machine on which you want to uninstall Operations Hub, select .
A list of programs that you can uninstall appears.
-
Right-click Operations Hub, and then select
Uninstall.
The
Uninstall Options screen
appears.

-
In addition to uninstalling Operations Hub, if you want to
delete all the related data and applications, select the
Purge databases during uninstall check
box.
-
Select Next.
The
You are ready to uninstall screen
appears.

-
Select Uninstall.
Results
Operations Hub is uninstalled from the Windows
machine.