Plant Applications Client

The Plant Applications Client provides a customizable environment for using Plant Applications views and displays to access plant data. Topics about the Client describe:

  • Setting up and managing the Client

  • Using the Client

TIP:  If you are using Windows Authentication and logging into a domain other than the default domain, you will need to include the fully qualified domain name (FQDN). Contact your site administrator if you need assistance.

Different Plant Applications modules enable different types of displays in the Plant Applications Client. Each display is also exposed as an ActiveX control. These displays can be used outside of the Plant Applications Client in any ActiveX container such as Intellution’s iFIX Workspace.

Details for the Plant Applications Client end-user configuration are stored on the server under the users’ log-on names. This provides the users with their own look and feel, no matter which computer they use.

Plant Applications Client sessions can be configured to time out and enter a protected state, thus requiring a user to log back in.  Refer to Configuring the Client Session Timeout.

Selected Plant Applications displays can be viewed through the Proficy Client installed by Proficy Workflow.  Plant Applications licensing is required.  Refer to Using Plant Applications Displays in the Proficy Client.

See also

Using the Plant Applications Client