Anatomy of a Sequence of Events (SOE) Display

Sequence of Event Displays are identified with the Sequence of Event icon . These displays interact with all event types, which can be sorted by time. Detailed information is provided for production, product change, and downtime, waste, and user-defined events. Key features of the screen are as follows:

  • The chronology of all events can be viewed in the left-hand window pane.

  • Sub-events can be viewed by clicking the event.

  • Detail for currently selected event in lower-right window. The display option, DisplayDetailPanel must be set to True to view the detail panel in the SOE display.

Key Uses

  • Review Downtime and Waste Events

  • Review Other Types of Events In Sequence with Downtime and Waste

  • Interact with Research Fields for Downtime and Waste

  • Enter User-defined Events

Key Data

  • All Data from Downtime and Waste

  • Research Fields for Downtime, Waste, User-defined Events

  • User-defined Event Times

  • User-defined Event Reasons

  • User-defined Event Comments

See Also

Adding User-defined Events

Modifying Event Details