Creating and Configuring a Schedule View Display

NOTE: This display is available only if you have purchased a Production license. To contact us, go to our Support site: https://digitalsupport.ge.com/.

Topics on using a Schedule View display are located in online Help for the Proficy Client, which is available on computers with the Client application installed.

To Create a Schedule View Display

  1. In the Plant Applications Server Manager tree, expand Client Management and then the Displays folder.

  2. Select a display group, then right-click on it and choose Add New Display > Schedule View.

  3. Enter the name of the new display. Display names must be unique.

  4. Select the new display, and then right-click on it and choose Edit (Display Name). Alternatively, double-click the display icon.

  5. In the Edit Display dialog box that appears, set the default time window of the display by updating the Initial and Max window hours.

  6. Enter a Max Edit time to limit the age of data that users may edit in this display.

  7. Click the Paths tab.

  8. Select each execution path from the list in Available Paths that will be used for this display, and then click Add.

  9. Click the Display Options tab. The various Schedule View Display Options can be used to enhance the functionality of the display.

  10. Click Save. Activate the display when prompted to do so.

  11. Click the Close button to close the Edit Display dialog box. The display is now available in the Plant Applications Client.

See also