Adding and Defining Production Statuses

  1. In the Plant Applications Administrator, expand Global Configuration

  2. Right-click Administer Production Statuses and select Edit Production Status. The Production Status Editor dialog box appears.

  3. Click New. The boxes become editable.

  4. In the Description box, type the name of the new production status.

  5. In the Status box, select the status that will indicate if this production status will be considered a state of Good or Bad production.

  6. In the Production box, select Yes if this is a status that will allow this event to be counted as production on this unit or select No if this status will not allow this event to be counted as production on this unit.

  7. In the Inventory box, select Yes if this is a status that will allow this event to be counted as production on this unit or select No if this status will not allow this event to be counted as production on this unit.

  8. Under Icon, select the desired flag color for this status.

  9. Under Color, select the desired color for this status.

  10. Click the check box to select the Bypass History flag to not record history for the chosen event status. Refer to Periodic Event Dimension Update.

  11. Click Save to complete the addition of the new production status.

See Also