Defining Valid Status Transitions

To Define The Valid Status Transitions

  1. Browse to the Plant Model and select the desired Production Line; right click and select Configure Execution Path from the menu.

  2. Select the Path Schedule tab.

  3. Select the Status Transitions tab.

  4. In the window named Status Transitions For This Path, click on a status in the far left window called Items With This Status.

  5. Set the Status transitions that are acceptable as transitions to and from this status in the Valid Transition window.  Move the Valid and Invalid Transition Statuses to the desired window using the various arrow buttons.