Creating Central-Level Specification Variables

The specification variable is the variable or quality test variable that is represented on a central or facility-wide basis. For example, the specification variables associated with the basis weight property could be BW, tear, tensile, burst, and so on.

To add a new specification variable

  1. Right-click on Specification Variables and click Add New Specification. An new entry text field appears.

  2. Type the name of the specification and press ENTER.