Exporting site users

Overview

You can export site users into an Excel workbook, and then use this workbook as a source file for importing site users into Plant Applications, either on the same server or on a different server. If you import the site users back into Plant Applications on the same server, you will need to edit at least one of the selected site user's fields in the workbook.

The following columns are automatically created during the export:

To export site users

  1. Log in to the Plant Applications Administrator application.

You must have Administrator access in the Administrator security group to export site users.

  1. Open Security Management.

  2. Right-click on the Site Users folder and select Export Site Users. The appears.

  3. Click the OK button.

  4. Plant Applications will automatically create the Excel workbook.

Once the workbook has been created, you can change any of the data in the worksheet and the use the worksheet to import the information into Plant Applications on the same server or on a different server.

See Also