Waste Distribution Charts by Units Web Part
The Waste Distribution Charts by Units Web Part displays the amount of waste for a specific period of time that is attributed to a specific location (unit), fault, reason level, product, and crew. Click the Table icon to display the information in a table format or click the Graph icon
to display the information as a bar chart.
The reporting time period is displayed at the bottom of the Web Part. To adjust the reporting period, click the Clock icon .
Terms
-
MAPE (Mean Amount Per Event): total waste amount/ number of waste events
-
MABE (Mean Amount Between Events): This is the mean amount that was produced between waste events.
To use this Web Part, you must first:
-
Configure your plant model. For more information on this topic, click here.
-
Capture waste events. For more information on this topic, click here.
-
Attach a reason tree to your waste events. For more information on this topic, click here.
-
Configure products and product changes. For more information on this topic, click here.
-
optional: Attach faults to your waste events. For more information on this topic, click here.
-
optional: Include crew/shift schedule information.
Waste Distribution Chart By Units (Bar Chart View)
When the Web Part is in Bar Chart view, each bar represents the total amount of waste assigned to a specific attribute, such as a reason. In Bar Chart view, you can click one of the bars to get a more granular view of your waste. For example, on the Location tab, you can click one of the bars for a specific location to view only the information specific to that location.
Waste Distribution Charts by Units Web Part (Table View)
In Table view, this Web Part provides the following information:
-
Location tab:
-
Location: This is a list of the location (unit) where the waste event(s) occurred.
-
Total: This is the total amount of waste for the specific location.
-
MAPE: This is the mean amount of waste for the specific location.
-
MABE: This is the mean amount that was produced between waste events for the specific location.
-
% Total: This is the percent total of waste attributed to the specific location.
-
# Events: This is the number of waste events that occurred at the specific location.
-
Totals: Totals are provided for the amount of waste for all locations and for the number of events for all locations.
-
Fault tab:
If no fault has been attached to the waste event, then the fault will be "Unspecified."
-
Fault: This is a list of the fault(s) assigned to the waste events.
-
Total: This is the total amount waste for the fault.
-
MAPE: This is the mean amount of waste for the specific fault.
-
MABE: This is the mean amount that was produced between waste events for the specific fault.
-
% Total: This is the percent total of waste attributed to the specific fault.
-
# Events: This is the number of waste events that occurred at the specific fault.
-
Totals: Totals are provided for the amount of waste for all faults and for the number of events for all faults.
-
Reason Level tab(s):
There will be a tab for each reason level in the associated reason tree.
-
Reason: This is a list of the reason(s) assigned to the waste events.
-
Total: This is the total amount of time attributed to waste for the reason.
-
MAPE: This is the total mean amount of waste for the specific reason.
-
MABE: This is the mean amount that was produced between waste events for the specific reason.
-
% Total: This is the percent total of waste attributed to the specific reason.
-
# Events: This is the number of waste events that occurred at the specific reason.
-
Totals: Totals are provided for the amount of waste for all reasons and for the number of events for all reasons.
-
Product tab:
-
Product: This is a list of the product(s) which were being run when the waste event(s) occurred.
-
Total: This is the total amount of waste for the specific product.
-
MAPE: This is the total mean amount of waste for the specific product.
-
MABE: This is the mean amount that was produced between waste events for the specific product.
-
% Production: This is the percent of total production that was waste.
-
% Total: This is the percent total of waste attributed to the specific product.
-
# Events: This is the number of waste events associated with the specific product.
-
Totals: Totals are provided for the amount of waste for all products, fault percent and number of events.
-
Crew tab:
-
Crew: This is a list of the Crew shifts when the waste event(s) occurred.
-
Total: This is the total amount of time attributed to waste for the specific Crew.
-
MAPE: This is the total mean amount of waste for the specific Crew.
-
MABE: This is the mean amount that was produced between waste events for the specific Crew.
-
% Total: This is the percent total of waste attributed to the specific Crew.
-
# Events: This is the number of waste events that occurred at the specific Crew.
-
Totals: Totals are provided for the amount of waste for all crews and for the number of events for all crews.
To configure the Waste Distribution Charts by Units Web Part
-
Create the web part. How?
-
On the Report Parameters tab, click the Edit Parameter button.
-
On the Units tab, select the units you want to include on this report.
-
On the Start Time and End Time tab, select the period of time for which you want waste information retrieved.
-
On the Options tab, select one or more of the following:
-
ProductFilter: Enter a product description or code to filter on that product.
-
-
On the Finish tab, click the Finish button to save your changes and to exit.
See Also