Alarm Count By Variables Web Part
The Alarm Count By Variables Web Part graphically displays the number and level of alarms during three user-specified time periods for selected variables. From this Web Part, you can view the Alarm List By Variables Web Part.
In order to use this Web Part, you must first:
Alarm Count By Variables Web Part
The top row indicates whether the number of alarms is trending up, down, or remaining the same. The alarm count for each category in the first row is compared to the alarm count for each category in the second row. For each alarm level, if the alarm count in the first row exceeds the alarm count in the second row, then a red down-pointing arrow is displayed. If the alarm count in the first row is less than the alarm count in the second row, then a green up-pointing arrow is displayed. If there is no change, then a green circle is displayed.
The red column displays the number of high alarms. The blue column displays the number of medium alarms. The yellow column displays the number of low alarms.
The first row of numbers is the number of alarms, in each category, for the specified Start Time #1. The second row of numbers is the number of alarms, in each category, for the specified Start Time #2. The third row of numbers is the number of alarms, in each category, for the specified Start Time #3.
You can click a number in the grid to open the Alarm List By Variables web part.
To create an Alarm Count By Variables Web Part
-
Create the web part. How?
-
On the Report Parameters tab, click the Edit Parameter button.
-
On the Variables tab, select the variables you want included on this web part.
-
After you've selected your variables, click the Start and End Time #1 tab. On this tab, you can specify the most current time period over which you want to count alarms on your selected variables. These alarm counts are displayed in the top row of the web part.
-
Click the Start and End Time #2 tab. On this tab, you can specify a time period prior to the time period specified on the Start and End Time #1 tab.
-
Click the Start and End Time #3 tab. On this tab, you can specify a time period prior to the time period specified on the Start and End time #2 tab.
-
Click the Finish tab and click the Finish button to save your changes and to return to the Web Part Administration dialog box.