Add a Lot to an In-Progress Work Order
Before you begin
To add a lot to a work order, all of the
following conditions must be met:
- The behavior Allow addition of material lots to a work order in progress is set for the route (see Create a Route Revision).
- The work order is in progress.
- The work order is for a serialized product.
- You have the permission to add lots to in-progress work orders running on the specified line (see About the Security Application)
Procedure
- Select the work order to modify.
-
Click
.
- Click Add Lots to Work Order. This will bring up the Add Lots to Work Order dialog.
- Enter the number of additional lots in NO OF LOTS TO ADD. This will add rows as required to the ENTER SERIAL/LOT# table.
-
Click
to generate the remaining SERIAL/LOT# and GENERATED SERIAL/LOT#.
-
Click ADD LOTS.
Added lots will be appended to the bottom of the list. There is no need to enter anything in the SERIAL/LOT# field; the Auto Populate function looks after this.