About the Status of a Serial/Lot and an Operation

The status of an operation indicates the progress of work for the operation.

The status of a serial/lot indicates the progress of work on the serial/lot for that specific operation. For example, suppose a work order includes performing operations 1 and 2. If operation 1 has been completed for a serial/lot, the status of the serial/lot for operation 1 is complete. If operation 2 is yet to begin on the same serial/lot, the status of the serial/lot for operation 2 is ready.

In the Work Queue application, the status of a serial/lot or an operation is automatically determined and displayed with a color-coded indicator. The following table provides a list of status indicators defined for a serial/lot and an operation.
Status Status Indicator Description for a Serial/Lot Description for an Operation
Not ready Not applicable Indicates that none of the serials/lots is available for you to perform the operation.
Cancelled Indicates that the work for the serial/lot has been cancelled. This happens if a defect has been created for the serial/lot, and the disposition provided in NCR Management is Scrapped. Not applicable
Ready Indicates that the serial/lot is available for you to perform the operation. Indicates that at least one serial/lot in the work order is available for you to perform the operation, and the operation is not in progress for any of the serials/lots.
Clocked on by you Indicates that the serial/lot is currently clocked on only by you for the operation. Indicates that at least one serial/lot in the operation is currently clocked on by you, and none of the serials/lots in the operation is clocked on by others.
Clocked on by another user Indicates that the serial/lot is currently clocked on by multiple users for the operation, but is not clocked on by you for the operation. Indicates that the serials/lots are currently clocked on by multiple users for the operation, but are not clocked on by you for the operation.
Clocked on by other users Indicates that the serial/lot is clocked on by multiple users for the operation, but is currently not clocked on by you for the operation. Indicates that the serials/lots are clocked on by multiple other users for the operation, but none of them are clocked on by you for the operation.
Clocked on by you and other users Indicates that the serial/lot is currently clocked on by you and other users for the operation. Indicates that the serials/lots for the operation are currently clocked on by you and other users.
Clocked on by other users in the past Indicates that work for the serial/lot has begun, but the serial/lot is currently not clocked on for the operation. Indicates that work has begun for at least one serial/lot in the operation in the past, but currently, no serial/lot is clocked on for the operation.
On hold Indicates that the serial/lot is on hold. This status indicator appears if a defect has been created for the serial/lot for the operation. After the defect is closed, the status is changed to the original status. Not applicable
Complete Indicates that the operation is complete for the serial/lot. Indicates that the operation is complete for all the serials/lots in the work order (or scrapped as applicable).
Skipped Indicates that the operation is skipped for the serial/lot. Indicates that the operation can be skipped.