You can add Historian
tags, Plant Applications variables, KPIs, process orders, batches, and golden batches to the
Analysis page to trend required charts and display tables for
analyzing information.
Before you begin
If you want to add Historian tags, you must provide the
Historian details:
- Install Historian Web-based Clients.
- Access the historian-config-prod.properties file. For
Enterprise Plant Applications, this file is located at
<installation folder of
Docker>/plantapps-web-docker/mnt/configfiles/historian-config/prod/1.1.0-SNAPSHOT
- For each Historian server whose tag data you want to add, provide the details of Historian as described in the following table.
Parameter |
Description |
Required/Optional? |
histN.service.origin |
The IP address, hostname, or the fully qualified domain
name (FQDN) of the machine on which you have installed Historian Web-based Clients. |
Required |
histN.service.port |
The port number on which the Historian Web-based Clients is running. |
Required only if it is other than 8443 |
histN.service.hostname |
The hostname of the Historian server, as configured in Plant Applications. |
Required |
histN.service.client_id |
The client ID of the Historian UAA service. The default value is admin. |
Required |
histN.service.client_secret |
The client secret of the Historian UAA service. |
Required |
histN.uaa.origin |
The IP address, hostname, or the FQDN of the machine on
which the UAA service used by Historian is
installed. |
Required |
histN.uaa.port |
The port number of the UAA service used by
Historian. |
Required |
hist.service.clientSecretEncrypted |
Indicates whether the client secret that you have
provided is encrypted. The default value is false. |
Required |
- Restart the following services:
- mesdataservice
- Processanalyserappservice
For Enterprise Plant Applications, these services are available as Docker
containers. For Standard Plant Applications, they are available as Tomcat
services.
Procedure
-
Log in to Plant Applications Web Client.
-
Select
.
The
Chart Configuration page appears. By default,
the
Tags option appears in the
Data
type list.
Note: After you login and select

for the first time, the default trend
chart appears. You can select

to go back to the
Chart Configuration page.
-
Select a context in the Plant Model list.
Note: You must expand the plant name to navigate and select the required
department, line, or unit of your plant. The selected department, line, or
unit appears for the plant model in the Plant Model
list.
-
Select the required Historian server in the Historians list.
Note: The Historians list appears only when you select
Tags in the Data type list.
You can plot the Historian tags belonging to multiple Historian servers, limited to 10 servers only. The Historian server can be local or remote. A local Historian server is installed on the same node as the Process Analyzer. The remote
Historian server is installed on a node different than that of the Process
Analyzer. The minimum supported version is Historian 7.0 SP5 or later.
-
In the Data type list, select one of the following
options:
- Tags
- Variables
- KPI (available for lines and units only)
- Process Orders (available only if Plant Applications Web Client is configured to use process orders)
- Batches (available only if Plant Applications Web Client is configured to use batches)
- Golden Batches (available only if Plant Applications Web Client is configured to use batches)
-
Depending on the data type, select one of the following options as shown in the
following table.
Data Type | Option |
---|
Variables |
Add Chart |
KPIs |
Add Chart |
Variables |
Add Chart |
Batches |
Add Batches |
Golden Batches |
Add Batches |
Process Orders |
Add Process Orders |
You can select multiple items.
Note: To add multiple items to an existing
chart, select Add Data for the chart. Alternatively,
to add a new chart, drag the required items to the Add
Chart button. GE recommends that you should restrict the
total count of tags or variables for Live charts to five to optimize the
trend chart output.
-
Select to select an interval from the available Presets or to select a custom
time interval by selecting the required dates and time, and then select
Apply.
The default time duration selected is the current time minus one hour. If
you select an interval from the calendar, the chart is enabled to be plotted
as the Historical chart instead of the Live chart.

-
After you add the required items to the charts, select
Plot.
With larger data samples the loading time of the analysis session may
increase.
A live chart is plotted on the screen as Chart 1.
Results
The Analysis
page appears, displaying the required trend charts and information.Tip: You
can select

to open the
Chart
Configuration page to search and add more tags, variables, KPIs,
batches, or process orders for analysis. In the
Chart
Configuration page, you can select

to
open the
Analysis page.
You can further save an
analysis trend to restore the analysis view. The trends you save are accessible by
all users. For more information, refer to the Save an Analysis Trend
topic.