Task List Filters
Users can perform context sensitive filtering in the Task List, which focuses a list of tasks or task steps on specific criteria.
Filtering Options for Tasks
The following table describes each available filter type.
Type | Value | Description |
---|---|---|
Task Name | User-defined |
Filter by text that is contained in the name of a task as well as searches using a wildcard character (*). |
Priority | User-defined |
Filter by the number that was assigned to the task when configuring the workflow, to indicate the task's priority for filtering purposes. The number(s) specified must be greater than zero. You can filter by multiple priority numbers by separating them with a comma, such as 1,2,3. You can also filter by a range of priority numbers, such as 1-5. These values are separated by a hyphen. If you want to filter by a series of ranges, you can separate them by commas (for example, 1-5, 10, 12-22).
Note: You can enter whole numbers only, such as 0, 1, 2, 3, and so on. |
My Task Steps | N/A |
Filter by the current operator's assigned task steps. Note: All task steps that have been acquired by another operator are hidden.
|
Task Step State | N/A |
Filter by the current state of an operator's assigned task steps.
|
Categories | N/A |
Filter tasks or task steps by a predefined grouping. |
Location Assignment | N/A |
Filters task steps by the equipment assigned to the task. |
Personnel Assignment | N/A |
Filters task steps by the person assigned to the task. |
Expiration | User-defined |
Filters tasks or task steps that expire within a defined time range (from now until a defined time), or by a specific date and time. If a task has an expiry, then this filter applies to the task. If the task step only has an expiry, then this filter applies to the task step(s). Note: If a task or task step expires while the filter is on, the task or task step will continue to be displayed in the Task List.
|