Associate a global subprocess with a task step template
Workflow designers create global subprocesses to be used as eSOP task step templates. You must first define the workflow subprocesses and configure the template options. Then, in Config Panels, you use task templates for additional, custom configuration.
Procedure
- In the navigator, click eSOP.
- In the Task Step Templates list, click Task Step Templates, and then click Add Task Step Template.
- In the Name and Description fields, enter a name and description for the resource.
- Click OK.
- Select the template you just created, or select an existing one.
- In the Displays panel, click Template Editor.
- In the Template Subprocess area, click Set.The Universal Browser appears.
- Select an existing subprocess, and then click OK.
- If you configured custom configuration panels that you want to add to this subprocess task step, perform one of the following actions.
Click this button... To... Add select an existing panel from Config Panels. Remove delete a selected panel from the table. move the selected custom panel to a higher level in the Task Editor, so that the tab of the custom panel appears closer to the standard tabs. That is, the tab moves further left. move the selected custom panel to a lower level in the Task Editor, so that the tab of the custom panel appears further from the standard tabs. That is, the tab moves further right. - Click Save.