Export server security certificates for an extension server
After installing the main application server in a multiple server environment, you must export the server security certificates and install them on your extension servers. During the extension server installation process, you must import these security certificates.
Procedure
- On the main server computer, click .The Export Workflow Application Server Certificates page appears.
- In the Export Folder field, enter the folder path or browse to the location where the certificates are to be exported.
- In the Password field, enter a password to secure the exported certificates, which will be used when importing the certificates to the extension servers.
- Click Save.A file with the extension .zip is created, which contains the certificates required on the extension servers.
- Click Exit.