Reassign personnel for a task stepReassign a person or a class to another task step

You can reassign a task step to a different person, as required, in the Task List.

Before you begin

Note: A workflow must be running to perform this action.

Procedure

  1. Log on to the Task List.
  2. If applicable, select the view you want to work in.
    Note: The default view is the Tasks tab.
    Click...To view...
    Tasksworkflow tsks currently being executed.
    Task Historycompleted tasks.
  3. Select the task that you want to work with.
  4. Click the task step that you want to work with.
  5. Click Actions.
  6. In the Task Step Actions section, click Personnel.
    The Universal Browser appears.
  7. Select the new user you want to assign this task step to.
  8. If an electronic signature is required, enter the appropriate information to authorize the action.
  9. Click OK.