Automated Calibration
About Automated Calibration
An automated calibration is one that is performed by using a calibrator. Calibration Management supports Fluke and GE Druck calibrators for automated calibration. It also supports automated calibration using the Beamex CMX calibration software.
Data Sent for Calibration
For each Calibration task, when you send calibration data to a Fluke Calibrator, a GE Druck Calibrator, or the Beamex CMX calibration software, information about the type of calibration that should be performed for an asset is exported. This information is stored in the Calibration Templates linked to the Asset records. These Asset records represent the asset that contain calibration measurements to be collected.
If you have sent calibration data to a Fluke Calibrator or a GE Druck Calibrator, the calibration data (i.e., the input values) are transferred to the calibrator.
For each calibration data that is sent to the Beamex CMX calibration software, a corresponding work order is created and stored in the folder path specified in the CMX Settings section in the Application Settings for Calibration Management. In the Beamex CMX calibration software, to represent the Hierarchy of the asset that will be calibrated, the Asset Hierarchy is created.
Data Received From Calibration
When you receive calibration data from a Fluke Calibrator, a GE Druck Calibrator, or the Beamex CMX calibration software, the results of selected calibrations are imported into GE Digital APM. After the data is imported, GE Digital APM will create one Calibration record for each calibration that you have selected, which appear as Calibration Events in the Calibration Events section. The Calibration records are populated with the values that you entered in the calibrator or Beamex CMX calibration software when you performed the calibration. You cannot save duplicate calibration data. If you saved calibration data twice in the calibrator, only one Calibration record is created in GE Digital APM after you receive data from the calibrator.
If you sent calibration data to a Fluke Calibrator, a GE Druck Calibrator, or the Beamex CMX calibration software, only those calibrations that were performed will be received in GE Digital APM. You must take the necessary action to complete calibrations that were not performed.
If you have received calibration data from a Fluke Calibrator or a GE Druck Calibrator, the fields in the Test Equipment section of the Calibration datasheet are populated with the details of the calibrator.
If you have received calibration data from Beamex CMX calibration software, the Calibration Passed field of the Calibration record is populated with a value to indicate whether the calibration passed or failed.
Supported Software and Devices
Device | Notes |
---|---|
CMX Calibration Management Software |
|
Fluke 744 / Fluke 754 Documenting Process Calibrator |
|
Fluke 729 Automatic Pressure Calibrator |
|
GE Druck Calibrator |
|
Verify Calibrator Settings for Fluke 74X - 75X or Fluke 729 FC
About This Task
Calibrator settings are saved for a user and for a data source. If you log in as another user, or change the data source, you must reconfigure the calibrator settings.
Procedure
What To Do Next
Verify Calibrator Settings for CMX
About This Task
Calibrator settings are saved for a user and for a data source. If you log in as another user, or change the data source, you must reconfigure the calibrator settings.
Procedure
What To Do Next
Verify Calibrator Settings for GE Druck
About This Task
Calibrator settings are saved for a user and for a data source. If you log in as another user, or change the data source, you must reconfigure the calibrator settings.
Procedure
What To Do Next
Send Data to a Calibrator
Before You Begin
- You can send Calibration data to a calibrator only if you are a member of the MI Devices Administrators Security Group.
- When you send data to a calibrator, the calibration data that already exists in the calibrator is deleted. Therefore, if you have data in the calibrator that you want to save, you must transfer the data to GE Digital APM.Note: You can activate the enhanced workflow on handling unsaved results and unfinished tasks in Fluke 74x - 75x and Fluke 729 FC Calibrators by selecting the Enable Fluke Task Management check box in the Admin section under Automated Calibration Settings tab. For more information, refer Fluke Task Management.
-
When you first try to send data to or receive data from the calibrator, if you have not installed the Meridium Device Service, you will be prompted to install it. This service must be installed on any machine that you will use with the calibrators.
Important: When a new device integration is introduced in the Calibration Management module, the Meridium Device Service utility is also modified to support the device. Therefore, if you have recently upgraded the GE Digital APM from an earlier version, you must uninstall the previous version of the Meridium Device Service utility, download the utility again, and then reinstall the downloaded version of the utility. - Verify the calibrator settings for Fluke, CMX, and GE Druck documenting process calibrators.
Additionally, to perform automated calibration by using the Beamex CMX calibration software, the following additional prerequisites must be fulfilled:
- Beamex CMX calibration software must be installed and running on the machine that you want to connect to the calibrator.
- Beamex Bridge software must be installed and running on the machine that you want to connect to the calibrator.
About This Task
This topic describes how to send Calibration data to a calibrator when performing an automated calibration.
You can perform manual calibration on tasks that use the Fluke 74X-75X template.
Procedure
What To Do Next
- Perform calibration using the calibrator.
- Receive data from the calibrator.
Receive Data from a Calibrator
Before You Begin
- Install the Meridium Device Service. When you first try to send data to or receive data from the calibrator, if you have not installed the Meridium Device Service, you will be prompted to install it. This service must be installed on any machine that you will use with calibrators.
- Verify the calibrator settings.
- Send calibration data to the calibrator.
- Perform the calibration on the calibrator.
- If you are using the Beamex CMX calibration software to perform automated calibration, the following additional prerequisites must be fulfilled:
- Beamex CMX calibration software must be installed and running on the machine that you will connect to the calibrator.
- Beamex Bridge software must be installed and running on the machine that you will connect to the calibrator.
About This Task
This topic describes how to receive data from calibrators that have been calibrated by using an automated calibrator.
Procedure
Fluke Task Management
About This Task
This topic describes how to activate enhanced Fluke Task Management workflow.
Procedure
Results
This setting provides the enhanced workflow during Send to Calibrator and Receive From Calibrator functionality for the following device types:
- Fluke 74x – 75x
- Fluke 729 FC
While performing Send Data to a Calibrator, the following check boxes appear if there are unsaved results and/or unfinished tasks found in the Calibrator.
- Save Results
- This check box is selected by default. If you select Next, then the unsaved results found in the Calibrator will be automatically saved into GE Digital APM. If there is any record that was sent to Calibrator and was modified or deleted in GE Digital APM before receiving the data from Calibrator or if the same result is uploaded twice then an error message appears while saving the results. In that case you need to navigate to the Receive From Calibrator screen and do the upload operation to review the errors.
- If you deselect this check box and select Next, then the unsaved results found in the Calibrator will not be saved into GE Digital APM. All the data in the Calibrator will be erased and newly selected tasks will be downloaded.
- Reload Unfinished Tasks
- This check box is selected by default and it indicates that the unfinished tasks found in the Calibrator will be reloaded back into Calibrator along with newly selected tasks.
- If you deselect this check box and select Next, then the unfinished tasks found in the Calibrator will not be reloaded and it will download the newly selected tasks.
- This check box is selected by default. If you select Finish, then all the results will be erased from the Calibrator and the unfinished tasks will be reloaded back to the Calibrator.
- If you deselect this check box and select Finish, then the results will not be erased from the Calibrator and the unfinished tasks will not be reloaded.
Data Validation Error Codes
Error Code | Description | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
CME00001 | Incorrect number of test points detected when compared to the template strategy. This is an error and the template will not be download to the Calibrator. The following are the possible causes of this error:
| ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
CME00002 |
Test point percentage values must be between 0 to 100. This is an error and the template will not be downloaded to the Calibrator. Test Point Percentage of one or more template detail records are outside the range of 0 to 100. Solution: Verify all template detail records and make sure the test point percentage values are between 0 to 100. | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
CMW00003 |
Primary Input or Output values are out of range. The selected device may not support this range of values. This is a warning. In this case, you can download the template to the Calibrator. However, you may not be able to perform calibration using the Calibrator. This is because, if the range values used in the template for Voltage, Current, Resistance, and Frequency are out of range, then the calibrator may not support this range. Solution: Modify the Input and Output range values in the template and make sure that the ranges entered are supported by Calibrator. | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
CME00004 |
Receive Mapping does not exist for the corresponding Send Mapping record of this template. You will not be able to upload the Calibration results back to APM. This is an error and the template will not be downloaded to the Calibrator. The following are the possible causes:
Solution: Restore the modified Send Mapping record. Make sure that a Receive Mapping record is available, whose Linked Mapping field is set to the template’s Send Mapping ID. | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
CME00005 |
Length of Tag Id value is greater than 30 characters which will be trimmed
This is a warning and the template will get downloaded. The following are the possible causes:
Solution: Modify the Tag Name field in the template to make sure that the length of the tag is within 32 characters. You can also modify the Location ID field in the calibration event record after saving the uploaded results in APM. | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
CME00006 |
Length of Tag Serial number is greater than 32 characters which will be trimmed. This is a warning and the template will get downloaded. The following are the possible causes:
Solution: Modify the Tag Serial Number field in the template to make sure the length is within 32 characters. You can also modify the Instrument Serial Number field in the calibration event record after saving the uploaded results in APM. | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
CME00007 |
The send mapping record is missing the following required field mappings
This is an error and the template will not get downloaded. The possible cause is that the following fields may have been deleted or modified in the Send Mapping record: Required field mapping for Analog template
Require Field Mapping for Discrete Template
Required Field Mapping for Functional Test Template
Solution: Restore the Send Mapping record and make sure the required field mapping exists before downloading the templates to the Calibrator. |