Supported Software and Devices

All GE Digital APM Components

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0

.NET Framework 4.7.2

and

.NET Core 3.1.1

APM System Monitoring

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0
MongoDB Community Edition

ASI for SAP

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0
SAP ECC 6.0 (Enhancement Packs [EhP] 1 through 8)

The following SAP system versions are required to update items in SAP with changes made in ASI:

  • To create ASI/ASM objects in SAP and import ASI/ASM objects from SAP: SAP ECC 6.0 - Enhancement Packs (EhP) 1 -8.
  • To update ASI/ASM objects in SAP:SAP ECC 6.0 - Enhancement Packs (EhP) 5 -8.
SAP S/4 HANA on-premises (1509, 1610, 1709, 1809, 1909, 2020) 

Calibration Management

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0

CMX Calibration Management Software Version 2 (2.10.114.0)

GE Device Driver 1.6.0.0

GE Digital APM Client Web Browser

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0

Google Chrome

New versions of Google Chrome are released every 4 weeks (schedule). Each version includes security updates, new features, and possible breaking changes. To ensure compatibility, GE Digital recommends that you use the latest Google Chrome version available. GE Digital APM V4.6.2.0.0 has been tested with Google Chrome version 96.

Microsoft Edge

New versions of Microsoft Edge are released every 4 weeks (schedule). Each version includes security updates, new features, and possible breaking changes. To ensure compatibility, GE Digital recommends that you use the latest Microsoft Edge version available. GE Digital APM V4.6.2.0.0 has been tested with Microsoft Edge version 96.

GE Digital APM Database

Supported Third Party ComponentsNotesGE Digital APM V4.6.2.0.0
Enterprise Edition or Standard Edition of Oracle Server 12.1, 12.2 or 12.2.03 (19c). In either case, Oracle Multimedia is required.

The GE Digital APM testing environment includes Oracle Server 12.1.0.1, 12.1.0.2, 12.2.0.1.0, and 12.2.0.3 (19c).

SQL Server 2016The GE Digital APM testing environment uses SQL Server 2016 SP1.
SQL Server 2017The GE Digital APM testing environment uses SQL Server 2017 RTM.
SQL Server 2019The GE Digital APM testing environment uses SQL Server 2019 RTM.

GE Digital APM Servers

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0
Windows Server 2016 Version 1607

GE Digital ActiveMQ Server

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0
Windows Server 2016 Version 1607
Note: The GE Digital APM testing environment uses Windows Server 2016 Version 1607.

GE Digital Redis Servers

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0
Ubuntu 18.04
Note: The GE Digital APM testing environment uses Ubuntu Server 18.04
Ubuntu 20.04
Note: The GE Digital APM testing environment uses Ubuntu Server 20.04.

Metrics and Scorecards

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0
Microsoft SQL Server Analysis Services 2014

OT Connect

Supported Third Party ComponentsNotesGE Digital APM V4.6.2.0.0
OT Connect OPC HDA Protocol AdapterTested internally with:
  • OSIsoft® PI Server version 3.4.390.16 with PI OPC DA/HDA Server version 1.2.7.0.
  • OSIsoft® PI HDA Server 2016, version 1.2.7.5.
OT Connect OPC DA Protocol Adapter
Note: The OPC DA Protocol Adapter is available with GE Digital APMV4.4.0.0.2.
Tested internally with:
  • OSIsoft® PI Server version 3.4.390.16 with PI OPC DA/HDA Server version 1.2.7.0.
  • OSIsoft® PI DA Server Server 2016, version 3.0
OT Connect OSI PI Protocol Adapter Requires Pi AF Client 2018 SP3 Patch 2.
Note: The OSI PI AF available with GE Digital APMV4.4.0.0.2.
Tested internally with:
  • OSIsoft® PI Server 2016 Asset Framework (AF), Version 2.8.
OT Connect GE Historian Protocol Adapter Requires Historian 7.2+ Client Access Assembly, targeting supported historian servers 4.0 and above.
Note: The GE Historian Protocol Adapter is available with GE Digital APMV4.4.0.0.2.
Tested internally with:
  • GE Historian 7.2
Note: The above information about OPC Servers and process historians are those that have been tested for the OT Connect feature.
Other OPC Compliant servers can also leverage OT Connect successfully, as OT Connect supports the following adapters:
  • OPC Foundation Historical Data Access (OPC-HDA) specification version 1.20, (AKA 1.2). The OPC HDA server offers the following capabilities:
    • LastReading
    • StartToEndReadings
    • SubscribeReadings
  • OPC DA Protocol Adapter that can connect to OPC Classic DA 3.0 servers. The OPC DA server offers the following capabilities:
    • LastReading
    • SubscribeReadings
  • OSI PI Protocol Adapter that can connect to PI Server 2010 and later through the Asset Framework (AF) Protocol. The OSI PI Protocol Adapter offers the following:
    • LastReading
    • SubscribeReading
    • GetStartEndReadings
    • GetBeforeEndReadings
  • GE Historian Protocol Adapter that can connect to Proficy Historian 4.0 and later through the Client Access API. The GE Historian Protocol Adapter offers the following Capabilities:
    • LastReading
    • SubscribeReading
    • GetStartEndReadings
    • GetBeforeEndReadings
The OT Connect Adapter can be installed and run on the OPC Server in CHECK MODE to validate the capabilities of specific OPC Servers and process historians on a case by case basis. Refer to the deployment section for more information on the OT Connect Adapter.
Note:
  • OT Connect does not support OPC PI Server Collectives.
  • To support direct consumption of Readings into Asset Health Indicators (AHIs) and triggered Policies, the server does need to implement the End aggregate.

Report Designer

Supported Third Party ComponentsNotesGE Digital APM V4.6.2.0.0
Microsoft Visual Studio 2017 ProfessionalNone
Microsoft Visual Studio 2019 ProfessionalNone
Microsoft SQL Server Data Tools - Business Intelligence for Visual Studio 2017 (15.8.0)
  • You can view a report designed using a lower version of Microsoft SQL Server Data Tools (SSDT) in a higher version of SQL Server Report Server (SSRS). However, you cannot view a report designed using a higher version of SSDT in a lower version of SSRS.
  • If you install SSDT for Microsoft Visual Studio 2019, install Microsoft Reporting Service Projects (VSIX 2.6.2). For more information on how to install Microsoft Reporting Services Projects (VSIX 2.6.2), refer to the Microsoft SSDT documentation.
Microsoft SQL Server Data Tools - Business Intelligence for Visual Studio 2019

Rounds

GE Digital APM ComponentsSupported Third Party ComponentsGE Digital APM V4.6.2.0.0
Rounds (iOS, Android and Windows tablet devices)Any operating system that meets the GE Digital APM Client operating system requirements.

Rounds Pro Mobile App

GE Digital APM ComponentsSupported Third Party ComponentsGE Digital APM V4.6.2.0.0
Rounds Pro Mobile App (iOS, Android and Windows tablet devices)Any operating system that meets the GE Digital APM Client operating system requirements.

R Scripts

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0
DeployR Open 8.0.0
Note: The GE Digital APM testing environment uses DeployR Open 8.0.0.
DeployR Enterprise 8.0.0
Note: The GE Digital APM testing environment uses DeployR Enterprise 8.0.0.
Machine Learning Server 9.2.1 or 9.3.0
Note: The GE Digital APM testing environment uses Machine Learning Server 9.3.0.

Rules

Supported Third Party ComponentsGE Digital APM V4.6.2.0.0
Microsoft Visual Studio 2017 or 2019 Professional
MSXML

SAP Interfaces

Supported Third Party ComponentsNotesGE Digital APM V4.6.2.0.0
SAP ECC 6.0 (Enhancement Packs [EhP] 1 through 8)None
SAP S/4 HANA on-premises (1509, 1610, 1709, 1809, 1909, 2020)
  • 2020: Support began from GE Digital APM V4.6.0.0.0
  • 1909: Support began from GE Digital APM V4.4.0.0.0
  • 1809: Support began from GE Digital APM V4.3.0.7.0
  • 1709: Support began from GE Digital APM V4.3.0.6.0
  • 1610: Support began from GE Digital APM V4.3.0.1 (Foundation), V4.3.0.3 added WMI and TC.
  • 1509: Support began from GE Digital APM V4.3.0.1 (Foundation) V4.3.0.3 added WMI and TC.

SQL Server Report Server

Supported Third Party ComponentsNotesGE Digital APM V4.6.2.0.0
Microsoft SQL Server Reporting Services 2014You can view a report designed using a lower version of Microsoft SQL Server Data Tools (SSDT) in a higher version of SQL Server Report Server (SSRS). However, you cannot view a report designed using a higher version of SSDT in a lower version of SSRS.
Microsoft SQL Server Reporting Services 2016
Microsoft SQL Server Reporting Services 2017
Microsoft SQL Server Reporting Services 2019

Supported Devices

Important:

Any management policy applied to mobile devices must be set up to allow the required permissions for the GE Digital APM mobile application. If restrictions are placed on iOS, Android, or Windows devices by a global policy or mobile device management system, then device storage, scanning, photography, location services, and other functionality may be disabled.

If you are using a Windows device, ensure that Windows App Store access is enabled.

Calibration Management Devices

DeviceV4.6.2.0.0
Fluke 74x Documenting Process Calibrator
Fluke 75x Documenting Process Calibrator
Fluke 729 Automatic Pressure Calibrator

GE Druck Calibrators:

  • Druck DPI611 - Pressure Calibrator
  • Druck DPI612 - Flex Pressure Calibrator
  • Druck DPI620 - Multifunction Calibrator
  • Druck DPI620-IS - Intrinsically Safe Multifunction Calibrator
  • Druck DPI620G – Advanced Multifunction Calibrator, HART/Fieldbus Communicator
  • Druck DPI620G-IS - Intrinsically Safe Advanced Multifunction Calibrator, HART/Fieldbus Communicator

*Calibration Management use the Devices Interface, which is a UI that is configured to support the transfer of data between GE Digital APM and devices that GE Digital APM supports.

Rounds Devices

DeviceNotesV4.6.2.0.0
Android, iOS, or Windows tablets that meets the GE Digital APM Client operating system requirements listed in the GE Digital APM Client requirements. None
Barcode Functionality
Device cameras for Android, iOS, and Windows tablets

This feature is available only when using the GE Digital APM mobile application.

Zebra TC-75X Touch Computer Integrated Barcode Scanner

Devices used in the GE Digital APM testing environment:

  • Zebra TC-75X Touch Computer (DataWedge version 6.4 or higher)
RFID Functionality
Zebra TC-75X Touch Computer NFC RFID reader

Device used in the GE Digital APM testing environment:

  • Zebra TC-75X Touch Computer (DataWedge version 6.4 or higher)

Rounds Pro Devices

DeviceNotesV4.6.2.0.0
Android, iOS, or Windows tablets that meets the GE Digital APM Client operating system requirements listed in the GE Digital APM Client requirements. None
Device cameras for Android, iOS, and Windows tablets

This feature is available only when using the Rounds Pro mobile application.

Zebra TC-75X Touch Computer Integrated Barcode Scanner

Devices used in the GE Digital APM testing environment:

  • Zebra TC-75X Touch Computer (DataWedge version 6.4 or higher)

Thickness Monitoring Supported Devices

DeviceV4.6.2.0.0
GE DMS Go
GE DMS Go+
GE DMS2
Olympus (Panametrics) 37DL Plus Ultrasonic Thickness Gage
Olympus (Panametrics) 38DL Plus Ultrasonic Thickness Gage

* Thickness Monitoring use the Devices Interface, which is a UI that is configured to support the transfer of data between GE Digital APM and devices that GE Digital APM supports.