Select Block
About this task
Description
A BCE Select clause of a Select …. Case statement. This block starts the statement. It must be followed by at least one Case Block and an End Select Block .
Parameters
This function block has the following parameter:
Parameter | Description |
Expression | An RCO Variable or any String or numeric expression. Strings must be in closed in double quotes. |
Example

The above function block uses a Select Block and all related blocks.
Procedure
- First, load tribute into an RCO Variable. For this example, the Attribute "COLOR" is loaded into RCO Variable 1.
- The next Select Block will perform a comparison on the contents of the RCO Variable. This example uses an RCO Variable, but any string or numeric expression will also work.
- The next block is a Case Block , and it is doing a comparison on "RED" and "GRN". If the RCO Variable contains either of these two values, then the function blocks immediately following the Case Block , up to the next Case Block , Case Else or End Select , will be executed. After the statements are executed, execution will jump to the block immediately following the End Select Block .
- The same operation will be performed on the next Case Block .
- The next block is the Case Else Block . The function blocks immediately following the Case Else Block are executed if none of the other Case Blocks in this statement evaluated to True.
- Finally, the End Select Block terminates the Select Statement .