What's New in CIMPLICITY 11
The HMI/SCADA CIMPLICITY v11.0 release includes the following new features and enhancements.
| Component | Feature Description |
|---|---|
| Alarm Setups |
|
| Basic Control Engine/ Scripting |
|
| CimEdit |
|
| CIMPLICITY |
|
| CIMPLICITY API tool kit |
CIMPLICITY supports Microsoft Visual Studio 2017. Note: Use Microsoft Visual Studio 2017 to recompile all programs that use APIs. |
| Database Logger | You can use the CIMPLICITY Database Logger to record a project's status log messages to the COR_LOG database table in addition to the cor_recstat.cl2 file in the project’s \log directory. |
| Points | The Change Approval UI has been enhanced to show the current value of the point being considered for change alongside the new value. |
| SCADA Web Configuration | You can now use CIMPLICITY's SCADA Web Configuration to discover the address space of an OPC UA Server and automatically create points from the address space. |
Note: Be aware of the following:
- Microsoft Access is no longer supported by CIMPLICITY.
- Portal is at its end of life, and its integration with CIMPLICITY is no longer supported. Contact your sales representative for alternate solutions.