Configuring the Correlation Statistics block

The window span and quality level through the following page:

  • Input 1 Fields: Lists the fields in input port 1.

  • Input 2 Fields: Lists the fields in input port 2.

  • Right list-box: Lists all the output fields. For each output cross correlations the field from input port 1 is listed in the Input 1 Fields column and the field from input port 2 is listed in the Input 2 Fields column.

  • Postfix: A postfix can be applied to or removed from all output field names.

  • Time Window Size: Shows the window span for the output field.

  • Quality level: Shows the quality level for the output field.  

Editing Actions
Buttons

  
Create output fields. Every selected field in port 1 is mapped with only 1 field from port 2. The number of fields selected from port 1 and port 2 must be the same.

 


Create output fields. Every selected field in port 1 is mapped with every selected field in port 2. This can generate a large number of outputs.

Change an output field's name

  1. Select the output field in the Output Fields column.

  2. Click on the field or press F2.

  3. Type the new field name.

Add / Remove a postfix to the output field name

  1. Enter the postfix in the PostFix edit box.

  2. Press "Apply to All" next to the PostFix edit box to append the postfix to each output field name.

  3. Press "Remove" next to the PostFix edit box to remove the postfix fromeach output field name.

    Note: Each of the ports adds their own postfix to the base name.

Change the time window span

  • Enter the desired time window size in the Time Window Size edit box.

Change the quality level

  • Enter the desired quality level in the Quality Level edit box.

Return to top


Related topics:

  

CSense 2023- Last updated: June 24,2025