Configuring the Cross Correlation block
The window span and quality level through the following page:
-
Input 1 Fields: Lists the fields in input port 1.
-
Input 2 Fields: Lists the fields in input port 2.
-
Right list-box: Lists all the output fields. For each output cross correlations the field from input port 1 is listed in the Input 1 Fields column and the field from input port 2 is listed in the Input 2 Fields column.
-
Postfix: A postfix can be applied to or removed from all output field names.
-
Time Window Size: Shows the window span for the output field.
-
Quality level: Shows the quality level for the output field.
Editing Actions
Buttons
Create output fields. Every selected field in port 1 is mapped with only 1 field from port 2. The number of fields selected from port 1 and port 2 must be the same.
Create output fields. Every selected field in port 1 is mapped with every selected field in port 2. This can generate a large number of outputs.
Change an output field's name
-
Select the output field in the Output Fields column.
-
Click on the field or press F2.
-
Type the new field name.
Add / Remove a postfix to the output field name
-
Enter the postfix in the PostFix edit box.
-
Press "Apply to All" next to the PostFix edit box to append the postfix to each output field name.
-
Press "Remove" next to the PostFix edit box to remove the postfix fromeach output field name.
Change the time window span
-
Enter the desired time window size in the Time Window Size edit box.
Change the quality level
-
Enter the desired quality level in the Quality Level edit box.
Related topics: