Configuring the Moving Sum block

Window Setup tab

  • Input Fields: Lists all the input fields.

  • Output Fields: Shows the output field name corresponding to the input field. You can edit the output fields, but the window span and quality threshold is read-only.

  • Window span: Shows the window span for the output field.

  • Quality level: Shows the quality level for the output field.

  • Change an output field's name

    1. Select the output field in the Output Fields column.

    2. Click on the field or press F2.

    3. Type the new field name.
       

  • Add / Remove a postfix to the output field name

    1. Enter the postfix in the PostFix edit box.

    2. Click "Apply to All" next to the PostFix edit box to append the postfix to each output field name.

    3. Click "Remove" next to the PostFix edit box to remove the postfix from each output field name.
       

Return to top

Time Window Configuration tab

Note: On the first execute, the block will read the value in the parameter field and lock on that value. The parameter value will not change during execution.

Change an output field's window span to a parameter field

  1. Select the input field that you wish to change. You can make multiple selections.

  2. Click on a parameter field that you want to use.

  3. Double click on the parameter field or click on the ">" button to update the selected window span(s).

Change an output field's window span to a fixed value

  1. Select the input field that you wish to change. You can make multiple selections.

  2. Change the window span edit box to the new value.

  3. Click on "Apply to selection(s)" to update the selected window span(s).

Apply the same fixed window span to all input fields

  1. Change the window span edit box to the new value.

  2. Click on "Apply to all" to update all the input field window span values with the new value.

Apply the same parameter window span to all input fields

  1. Click on a parameter field that you want to use.

  2. Click on the ">>" button to update all the input field window span values with the parameter field.

Quality Threshold Configuration tab

Change an output field's quality level to a parameter field

  1. Select the input field that you wish to change. You can make multiple selections.

  2. Click on a parameter field that you want to use.

  3. Double click on the parameter field or click on the ">" button to update the selected quality level(s).

Change an output field's quality level to a fixed value

  1. Select the input field that you wish to change. You can make multiple selections.

  2. Change the Quality Threshold edit box to the new value.

  3. Click on "Apply to selection(s)" to update the selected quality level(s).

Apply the same fixed quality level to all input fields

  1. Change the quality level edit box to the new value.

  2. Click on the "Apply to all" button to update all the input field quality level values with the new value.

Apply the same parameter quality level to all input fields

  1. Click on a parameter field that you want to use.

  2. Click on the ">>" button to update all the input field quality level values with the parameter field.

Reurn to top


Related topics:

  

CSense 2023- Last updated: June 24,2025