Proficy Historian Sink block

The Proficy Historian Sink block accumulates field data in an existing Proficy Historian. During execution all fields that do not exist in the historian will be created. The value and quality will be written to the historian on every execution timestamp. If an entry for the given timestamp and field does not exist, a new entry will be created otherwise the existing value will be updated.

Note that this connector may or may not be available on the user palette, according to your license type.

Return to Overview of blocks

Proficy Historian Sink BLOCK

Block Type

Input/Output block

Input/Output ports

The Proficy Historian Sink has no output ports and one input port.

Functions performed on tags

This block performs no functions on the input data, it simply writes the data, for the configured tags, that it receives from the Blueprint to the historian.  


Related topics:

  

CSense 2023- Last updated: June 24,2025