Reset on Input Change block

Generates a reset event when the input changes. This block is used in conjunction with blocks that can handle the reset event.

Return to Overview of blocks

Reset on Input Change block

Description

Generates a reset event when the input changes. This block generates a reset event for blocks able to handle a reset event.  The reset event can pass a time stamp to the block that is being reset.  This time stamp may either be the current execution time stamp or may be read from the input to this block. In both these cases it is possible to compensate for local time by means of an offset.

Diagram showing the reset on input change block

Block Type

Time based block

Input/Output ports

The input port must be connected to a port that only has 1 field. The field may be of any type.

Blocks that handle a reset event

Return to top


Related topics:

  

CSense 2023- Last updated: June 24,2025