Troubleshooting the PLS Model block

Return to:

PLS Model block

Configuring the PLS Model block

Design Time Runnability

ERROR REPORTED

ACTION REQUIRED

No PLS model loaded.

Load the XML file of the PLS model.

All of the model input fields are not mapped to the data source input fields from the Input port.

Map the model fields to the input data fields.

Run-Time

ERROR REPORTED

 ACTION REQUIRED

WILL IT STOP THE BLUEPRINT?

One of the input fields gives a different value or quality for the same timestamp in two consecutive executes.

Check your solution blueprint for any changes made to the timestamp. If data values are changed at all, the timestamp must be changed, and the timestamp must have increased from the previous one.

Yes

The timestamp of one of the input fields for an execute is older than the timestamp for that field on the previous execute.

Check your solution blueprint for any changes made to the timestamp. If data values are changed at all, the timestamp must be changed, and the timestamp must have increased from the previous one.

Yes

 

 

 

 

 

 

  

CSense 2023- Last updated: June 24,2025