Overview of blocks

A Block is a unit that performs a calculation in a blueprint.

In this section you can view all the blocks within Architect:

Input

There is a growing list of interfaces.

The OPC Classic client and server blocks are the workhorse interfaces. Architect provides other custom interfaces as well.

Return to top

Output

General

General blocks for managing the flow of information.

The Superblock allows the user to organize solutions hierarchically (a Superblock contains other blocks).

Return to top

Rules & Models

Provides for:

  • Data-driven modeling techniques such as nonlinear models and linear models

  • Knowledge-driven modeling techniques, such as fuzzy logic or scripting

The COM and .NET wrapper blocks enables the user to add existing code (e.g. in VB, C++, Delphi, etc.), applications, or any functionality not directly supported by Architect. They also enable adding custom blocks to Architect, as long as these custom blocks adhere to the specified COM or .NET interfaces.

Statistical

Time-based

These blocks are useful for dynamic processes with time delays (fixed or variable), or with sample values that become available only later, for example.

Return to top

Mathematical

Blocks for mathematical functions. The rate of change and limiter blocks are especially useful from a data quality and data validation perspective.

Return to top

Data Transformation

Transform your data to a more usable format. Some examples include using the String lookup block to convert event codes to string messages, or the Limit switch decoder block to correct the signals from a pair of limit switch signals for an instrument such as a valve.

Return to top

Data Quality

Each block in Architect has data quality as a property, which is very important in providing a reliable solution. It is also critical for developing proper and reliable data-driven models.

Return to top

User blocks

User blocks contain a reference to an external file which are pre-configured blueprints and/or superblocks that have been created according to specific requirements, and are saved as .cub files.  

Template blocks

User blocks contain a reference to an external file which are pre-configured blueprints and/or superblocks that have been created according to specific requirements, and are saved as .cut files. When a blueprint contains template blocks, the external file is not loaded into the current blueprint until the blueprint is expanded.

Common Analytics Framework (CAF) blocks

Each block on the CAF palette represents a different Analytic that can be used in a blueprint. Each Analytic will have specific configuration requirements in order for the Analytic algorithms to be calculated.


Related topics:

  

CSense 8.5 SP1- Last updated: July 09,2025