ihuRetrieveCalculatedDataEx
Prototype
Use the ihuRetrieveCalculatedDataEx
function to return calculated data based on the raw samples stored in the archive. Average
, Minimum
, and Count
are example CalculationMode
values.
ihuRetrieveCalculatedDataEx {
long serverhandle, // [in] which server to fetch from
IHU_TIMESTAMP StartTime, //[in] Start time of query
IHU_TIMESTAMP EndTime, //[in] End time of query
ihuCalculationMode CalculationMode, //[in] Calculation Mode
unsigned long NumberOfSamples, //[in] Number of samples to be returned
IHU_DATA_INTERVAL Interval, // [in] Interval in Milliseconds
IHU_RETRIEVED_DATA_RECORDS_EX *DataRecords //[in/out] - you fill in tagnames of the structures and API will fil
};
Remarks
To request data, you can specify a number of samples or a time interval. Set one parameter to a non-zero value and the other to 0
. To split the duration, divide the time from start to finish into evenly spaced time intervals.
Returns
The ihuReadRawDataByTimeEx2
function returns ihuSTATUS_OK
when values are successfully retrieved, and returns errors on:
- Read timeouts
- User is not a member of the ih Readers security group
- Tag not found