Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Verifying the Syntax of a Calculation Formula
About this task
Perform a syntax check to make sure that your formula is constructed correctly and executes. The syntax check does not identify invalid (misspelled or deleted) tagnames in the dependency list. It does not check all branches of a calculation; it only tests the calculation formula based upon the logic and current values. It also may not return the same result as the collected value.
Procedure
In the Tag Maintenance screen, from the Calculation tab, select the Test button.
The dialog box shown in the following figure appears, with a Value and Quality statement confirming there are no errors.
If you have a syntax error, a dialog appears detailing the error, as shown in the following figure.