Proficy Historian Client Access API
Proficy.Historian.ClientAccess.API Namespace / VersionHeaderBehavior Class
Members


VersionHeaderBehavior Class
Syntax
Public Class VersionHeaderBehavior 
   Inherits System.Attribute
Inheritance Hierarchy

System.Object
   System.Attribute
      Proficy.Historian.ClientAccess.API.VersionHeaderBehavior

Requirements

Target Platforms: Windows 7, Windows Vista SP1 or later, Windows XP SP3, Windows Server 2008 (Server Core not supported), Windows Server 2008 R2 (Server Core supported with SP1 or later), Windows Server 2003 SP2

See Also