Important: You do not have the latest version of Historian! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Historian product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Optimize the Server Performance
About this task
If the file sharing and printer sharing options on the computer on which you want to install Historian is set to maximize data throughput, it can lead to excessive paging when dealing with large files, which can interfere with applications like Historian. This topic describes how to change these settings to optimize the performance.
Procedure
Access the Control Panel.
Double-click Network and Dial-Up Connections.
The Network and Dial-up Connections window appears.
Right-select Local Area Connection Properties, and select Properties.
Select File and Printer Sharing for Microsoft Networks, and select Properties.
Ensure that the Maximize Data Throughput for Network Applications option is selected.