The Generate Wizard lets you add many similar blocks to the database quickly, saving development time. You simply select the type of block you want to create and the block names you want to use. For the block type, you can select an existing or a new block. This selection determines the specific values assigned to each block created. For example, when you select a new block, the Wizard creates blocks with default values. However, when you select an existing block, the Wizard creates blocks with values of the selected block. This option lets you create many similar blocks quickly without having to reconfigure them later. When specifying the block names, you must enter a prefix, suffix, starting number, ending number, and increment value. The Generate Wizard uses this information to systematically assign names to the blocks it creates. For example, the following values create blocks with the names F1T1 through F20T1.
The Generate Wizard cannot create a block with a name that already exists. If the information you specify results in an existing block name, the Wizard skips that block and continues on to the next one. Using the Generate Wizard, you also have the option of customizing up to 5 fields. Customizing these fields lets you fine tune the block's configuration. For example, if you need to create 50 Digital Input blocks, each one will have a different I/O address. You can use the Generate Wizard to assign these addresses if they occur in a sequential order. You can customize a field by selecting it and entering a prefix, suffix, starting number, ending number, and increment value. The Wizard handles this information identically to the block name values you entered. If the resulting sequence of field values ends before the Wizard creates all the new blocks, the sequence repeats from the beginning. For example, suppose you want to create 10 Analog Input blocks, AI1 through AI10 and you customize the I/O address of each block with the following information:
The blocks receive the following addresses:
You also have the option of enabling the Use Custom Format check box. When you enable this check box, the Wizard lets you enter multiple patterns for the five fields you have selected. A pattern acts as a programming statement for generating a range of numeric or string values. The following table lists the syntax for each type of pattern. Notice that the difference between literals and constants is minor. Both are strings and can be up 40 characters. However, quotation marks (" ") are required for constants when the string contains any mark of punctuation or non-alphanumeric symbol such as an angle bracket or a colon. If the string contains only numbers or letters, the quotation marks are optional. Also notice that negative and floating point numbers are not supported within patterns. You can generate these types of numbers by enclosing a minus sign or a decimal point in quotation marks outside of the pattern. Negative increments are not supported. Consider the following examples:
By combining different pattern types, you can generate a wide range of block field entries. For example, if you want to customize the Description field for a group of blocks, you could enter a pattern such as Alarm Status from Area <"A", "B", "C">. Notice that the text outside the pattern does not require quotation marks.
See AlsoHow Do I... |
Important Notice You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the iFIX product page. For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com. For the most up-to-date documentation, go here. |
![]() |