Moving Blocks

In addition to sharing blocks by copying and pasting them, you can cut and paste them. Cutting blocks from the database is similar to copying them; the main difference is that cut blocks are physically moved and placed on the clipboard, allowing you to move blocks to other databases.

Prior to removing blocks from their chains, Database Manager takes each chain off scan. Make sure you place the chain on scan when you finish editing it. iFIX provides several ways to do this. For more information about placing a block or chain on scan, refer to the section Placing Blocks On and Off Scan.

If you cut a block from the middle of the chain, Database Manager attempts to connect the two portions of the chain, as the following figure shows.

Removing a Block from a Chain

 

See Also

How Do I...

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.