iFIX Background Tasks

iFIX starts and stops background tasks based on the configuration information in the SCU file. The table below describes the function of each iFIX background task. Automatic tasks are started by iFIX if required by your configuration. Tasks listed as optional require that you start them manually by adding them to the configured task list in the Task Configuration dialog box in the SCU.

NOTE: If you want, you can configure certain tasks to start up automatically. Refer to the Configuring Startup Tasks section for more information.

System Tasks 

Program

Executable File

Function

Alarm File Task (Automatic)

ALMFILE.EXE

Receives alarm messages and stores them in files.

Alarm Printer Task (Automatic)

ALMPRIN.EXE

Receives alarm messages and sends them to printers.

Alarm Summary Task (Automatic)

ALMSUM.EXE

Receives alarms for display in the iFIX WorkSpace through the Alarm Summary object.

Alarm Manager (Automatic)

NAM.EXE

Distributes alarm messages over the network. Alarm managers run on SCADA servers.

Alarm Client (Automatic)

NAC.EXE

Receives alarm messages over the network.

Historical Collect (Optional)

HTC.EXE

Collects data according to the Historical Assign configuration file.

I/O Control (Automatic, SCADA)

IOCNTRL.EXE

Starts the I/O drivers, and displays the status of the installed I/O drivers running on the SCADA server.

Summary Queue Delete (Automatic, SCADA)

SUMQDEL.EXE

Removes the acknowledged, returned to normal, alarms from the Alarm Summary queue.

Scan Alarm and Control (Automatic, SCADA)

WSACTASK.EXE

Updates the database with data from the I/O driver, makes requested writes to the I/O Driver, generates alarms, and executes the logic of the database chains.

Network Diagnostics (Optional)

NETDIAG.EXE

Displays the status of sessions on the local node.

TCP/IP Task (Automatic)

TCPTASK.EXE

Supports node-to-node communication over TCP/IP.

Node Name Table (Automatic)

NNTABLE.EXE

Stores network information about the local and remote nodes.

Connection Manager (Automatic)

CONMGR.EXE

During startup, establishes the sessions listed in the configuration file. Monitors the status of sessions on the local node and generates alarm messages if sessions go down. It also attempts to re-establish sessions that have gone down.

Alarm ODBC Service (Automatic)

AlmODBC.EXE

Reads alarms and messages generated by iFIX and logs them to an ODBC-compliant database.

Event Scheduler (Optional)

FixBackgroundServer.EXE

Runs time and event-based scripts, allowing you to schedule reports and monitor events.

Workspace (Optional)

Workspace.EXE

Opens the iFIX WorkSpace where you can open, edit, or view pictures.

For information on command line parameters available for starting the WorkSpace in run mode, refer to the Command Line Parameters for Starting the iFIX WorkSpace section.

 

See Also

How Do I...

Important Notice

You do not have the latest version of iFIX! You are missing out on the newest capabilities and enhanced security.

For information on all the latest features, see the iFIX product page.

For more information on upgrades, contact your GE Digital sales agent or e-mail GEDClientServices@gevernova.com.

For the most up-to-date documentation, go here.